Brand Colors — Emerson
Brand Primary
#00573d
Brand Primary Hover
(base lightened 8%)
#00805a
Brand Secondary
#004b8d
Brand Colors — Greenlee
Brand Primary
#7ac436
Brand Primary Hover (base darkened 8%)
#66a42d
Brand Secondary
#2d383f
Brand Colors — Klauke
Brand Primary
#004494
Brand Primary Hover (base darkened 8%)
#00316b
Brand Secondary
#2d383f
Brand Colors — ProTeam
Brand Primary
#6a37b0
Brand Primary Hover
(base darkened 8%)
#572d91
Brand Secondary
#f6cf3f
Brand Colors — RIDGID
Brand Primary
#da291c
Brand Primary Hover
(base darkened 8%)
#b62217
Brand Primary Alt
(Licensed Products)
#f88126
Brand Primary Alt Hover
(base darkened 8%)
#ed6b08
Brand Secondary
#2d383f
Brand Tertiary
#004b8d
Brand Colors — Workshop Vacs
Brand Primary
#f0b310
Brand Primary Hover
(base darkened 8%)
#ca970d
Brand Secondary (Emerson Grey)
#9fa1a4
Global Colors — Base Palette
Base
(Grey Dark 48)
#262728
Base Alt
(Grey Dark 56)
#121313
Base Reverse
(Grey Light 40)
#ffffff
Base Error (Red)
#d31245
Base Warning (Amber)
#f8b11e
The Global Base Color Palette is to be shared across all Emerson digital properties and intended to ensure consistency for all basic content UI such as text elements (color options for both light & dark backgrounds), form errors and warning notifications. Utilizing these colors globally across sites and applications will ensure all brands are consistently promoting appropriate contrast standards and readability best practices.
Global Colors — Grey Scale Palette
Grey Light 40
(Base lightened 40%)
#ffffff
Grey Light 32
(Base lightened 32%)
#f3f3f3
Grey Light 24
(Base lightened 24%)
#dedfe0
Grey Light 16
(Base lightened 16%)
#c9cacc
Grey Light 8
(Base lightened 8%)
#b4b6b8
Emerson Grey
(Base)
#9fa1a4
Grey Dark 8
(Base darkened 8%)
#8a8c90
Grey Dark 16
(Base darkened 16%)
#75787c
Grey Dark 24
(Base darkened 24%)
#626467
Grey Dark 32
(Base darkened 32%)
#4e4f52
Grey Dark 40
(Base darkened 40%)
#3a3b3d
Grey Dark 48
(Base darkened 48%)
#262728
Grey Dark 56
(Base darkened 56%)
#121313
Grey Dark 64
(Base darkened 64%)
#000000
The Global Grey Scale Palette is to be shared across all Emerson digital properties to convey a sense of unity between distinctive brand identities. The palette is a programmatically generated range of values based on the Emerson Grey brand color and provides a full spectrum of value options from white (Grey Light 40) to black (Grey Dark 64). If any changes to the base grey are needed in the future, updating the hex value of Emerson Grey will cascade across the palette without requiring additional effort to update the other values.
While intended primarily for use with presentation UI elements, such as component backgrounds, content dividers, borders, and other visual elements used to designate or separate distinct blocks of content, the palette provides a number of values that may be suitable for some secondary content elements as well. These may include supporting content such as subtext & microcopy, author bylines, date/time stamps, category labels, etc. as appropriate for the given use case.
Global Colors — Accent Grey Palette
Blue Grey
#dee6ea
Cool Grey
#c4ced1
Cool Grey Hover
(base darkened 8%)
#adbbbf
The Global Accent Grey Palette includes existing colors currently in use on the on the Emerson.com site and elsewhere that are not part of the new programmatic grey scale palette. Some use cases for these legacy colors include Secondary & Tertiary CTA buttons, tab component backgrounds, table cell highlighting & interaction states, etc.