An alternative layout version of the H008B, this hero is used to feature heading content for a press releases, case studies or other stylized article content.
Created primarily for use on press release pages, the H008C is an alternative version of the H008B hero intended to be used at the top of an article page. Similar to its B version, this hero variant features offset header copy consisting of a category descriptor (“eyebrow”) label, headline and subhead (optional), but also includes an optional left-aligned feature image that can be accompanied by an image caption and link text.
The H008C was designed to keep offset header content aligned with the left edge of article body copy below when arranged in a 2-column layout using a C044 Rich Text Wide component. However, this hero may alternatively be used with article content arranged in single-column layouts using the C034 Rich Text component as well.
Image caption may optionally include a link to download a high-resolution version of the image asset displayed.
Eyebrow Label: 40
Heading: 90
Subhead: 120
Image Caption: 200
Asset Size: 600px x 450px
Asset Aspect Ratio: 4:3
Recommended File Weight: <100kb
Width: 400px
Height: 272px
Desktop: 4:3
Tablet: 4:3
Mobile: 4:3