Usage Guidelines
When To Use:
Utilize to lead to the country locale in order to drive to other documents/web pages.
When To Avoid:
When you don’t have tabular data or lists that need stylized grouping.
A component built of multiple C053 Table Group and C052 Row Group sub-component items used to display nested tables in a 2-column orientation.
Usage for the interim language selector page leads to the country local, or when re-purposed for other uses can drive to documents or web pages.
These tables are typically used on language selector page. Can be used in place of the C027 Table when two columns of tabular data are preferred.
**Note: The C054 component must consist of at least one C053 Table Group (a 1-column grouping with a group heading and table content), which in turn must consist of one or more C052 Row Groups (a 2-column grouping of item label and data). C052 and C053 are sub-components only and cannot be used as standalone components outside of a C054 parent wrapper.
Authoring of this component can be somewhat complex due to its sub-component requirements. Consult the CMS Authoring Guide for more information on how to build this table.
Links lead to the country locale or when re-purposed for other uses can drive to documents or other pages.
Headline: 50-75
Body Copy: No limits, but consider the impact of the visuals when using this table
Utilize to lead to the country locale in order to drive to other documents/web pages.
When you don’t have tabular data or lists that need stylized grouping.