Usage Guidelines:
When to Use:
When you need to show data in tabular form
When to Avoid:
When you have information that is better suited by plain text as opposed to columns and rows
Alternative Options:
N/A
Three types of static tables are available and should be used on a case-by-case basis depending on the intent of the table’s design.
Tables are currently available in the Generic Details layout (L022) and Case Study layout (L026). There are currently three types of tables available at this time: two Responsive versions (re-flow and overflow), and a version that opens in a new window or tab to make the table more readable in cases where the table is not responsive. These options will be used on a case-by-case basis depending on the table’s content.
This is a static component that does not have calls to action.
Headline: 100
Column Headers: 60 (30 X 2 lines)
Row Headers: 60 (30 X 2 lines)
When you need to show data in tabular form
When you have information that is better suited by plain text as opposed to columns and rows
N/A