The Local Selector Utility Modal allows visitors to select which country and language version of the site they would like to see.
The component features a typeahead text entry box for Country/Region selection which will display available languages. Languages can be selected via a radio button.
Choosing a Country/Region and language and selecting the “Select” CTA button will direct the user to the associated site locale and also update their Localization Cookie, returning them to the same locale when they navigate back to Emerson.com.